Cut, copy, and paste project elements
Cut, copy, and paste elements in the
System
explorer to remove or reuse FactoryTalk Smart Objects, programs and routines.To cut, copy, and paste project elements
- On the explorer bar, select
System. The elements in the project appear. - InSystem, select a FactoryTalk Smart Object, or expand the FactoryTalk Smart Object to select a program or routine.
- SelectEdit > CutorEdit > Copy.
- Select the location to place the element and selectEdit > Paste. The element and the content within the item appear in the new location.TIP:
- Copying and pasting elements increments element names numerically.
- Valid paste operations include:
- Pasting a FactoryTalk Smart Object in another FactoryTalk Smart Object or in the blank space at the bottom of the explorer pane.
- Pasting a program in a FactoryTalk Smart Object.
- Pasting a routine in a program.
- To use the menubar or keyboard to perform operations:
- SelectEdit > Cutor pressCtrl+X.
- SelectEdit > Copyor pressCtrl+C.
- SelectEdit > Pasteor pressCtrl+V.
- Menu options are unavailable when you cannot cut, copy or paste the selected elements.
- An error message appears when you attempt to use a keyboard shortcut for an invalid operation.
Provide Feedback