Open the code editor
Open the code editor to view and edit the code for
FactoryTalk Design Studio
elements.
IMPORTANT:
Changing the name of any object using the code editor does not change all references to that object.
To open the code editor:
- InFactoryTalk Design Studio, open a routine.
- Select
Code editorto open the code editor.
You can also right-click an element and open the code editor:
- In theExplorerpane, select
System,
Devices,
Execution, or
Libraryto display elements. - Right-click an element and selectCode editor.
Provide Feedback