View messages for the tags and logic in the project
View error, warning, and information messages for the logic in your project. The
Messages
tab allows you to go to the location associated with the message and correct the issue. You do not have to open the routine to review messages. - If theOutputpane does not appear, in the pane bar, select
Outputor selectView > Output > Messages. - InOutputunderMessages, select the option to view the desired messages:
- Entire project. View messages for the entire project. This is the default.
- Current tab. View messages for the current tab in focus.
- InDescription, read the description of the message.
- InLocation, select the link to open the location in the routine so that you can resolve the issue.TIP: To sort by location, select theLocationcolumn header to toggle between ascending and descending order.
- (optional) InSearch, type a portion of the description or message.Messagesreturns rows that meet the search criteria.
- Select theErrors,Warnings, andMessagesbuttons to filter the display to show those message types. Each button indicates the message count for that type.

Provide Feedback