Toolbar
Icons in the toolbar include:
Icon | Description |
|---|---|
Device list . Opens the Device list to view and set controller and device properties. | |
Commit . Save changes to the local repository. | |
![]() | Push . Transfer commits from the local repository for the shared project to the remote repository. The number in the icon identifies the total commits made by the current user (local commits). |
![]() | Pull . Update the local repository of the shared project from the remote repository. The number in the icon identifies the total commits made by other users sharing the project (remote commits). |
The Change history tab shows all changes committed to the repository for a local or shared project. |
Provide Feedback