Configuration Tag definitions
The following table lists the available configuration tags.
Name | Data Type | Definition | Valid Values | |||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|
Axisxx.MotorCurrent | SINT | Specifies the continuous current that is supplied to the motor when
the motor is moving. | 0.1…4.0 A | |||||||||
Axisxx.HoldCurrentPct | SINT | Specifies the percentage of motor current to apply to maintain
holding torque while the axis is stationary. | 0…100% | |||||||||
Axisxx.Microsteps | INT | Determines the number of microsteps that is equal to one full motor
step. | 1, 2, 4, 8, 16, 32, 64, 128, and 256 microsteps | |||||||||
Axisxx.StepsPerRevolution | INT | Determines the number of full steps per motor revolution. |
| |||||||||
Axisxx.VelocityProfile | SINT | Determines the acceleration and deceleration profile to use for
motion commands. |
| |||||||||
Axisxx.UnitsPerRevolution | REAL | Engineering Units per revolution. Position, speed, and rate of change parameters are divided by this
value to convert them from Engineering Units to Revolution. | Any positive value | |||||||||
Axisxx.MaxSpeed | REAL | Specifies the maximum speed that the axis is allowed to move. If the commanded velocity exceeds maximum speed, the actual velocity
is limited to maximum speed and I.Axisxx.OverspeedAlarm is set to
1. The value is in Engineering Units per second. | Any positive value | |||||||||
Axisxx.JogAccel | REAL | Specifies the speed's rate of change for the Jog command. The value is in Engineering Units per second 2 . | Any positive value | |||||||||
Axisxx.InvertDirection | BOOL | Determines whether to invert the logical motor direction to account
for installation or mechanical orientation differences. |
| |||||||||
Axisxx.InvertHomeInput | BOOL | Determines whether to invert the input trigger for the Home Limit
Switch. This configuration does not affect the behavior of O:HomeSwitch. |
| |||||||||
Axisxx.InvertPositiveOvertravelInput | BOOL | Determines whether to invert the input trigger for positive
overtravel. This configuration does not affect the behavior of
O:PositiveOvertravel. |
| |||||||||
Axisxx.InvertNegativeOvertravelInput | BOOL | Determines whether to invert the input trigger for negative
overtravel. This configuration does not affect the behavior of
O:NegativeOvertravel. |
| |||||||||
Axisxx.HomeType | SINT | Determines the method that the axis uses to detect the home position
in a Home operation. | 0 = Home Limit Switch The Home Limit Switch is connected to local digital input or external
digital input (Detection is triggered using
O.Axisxx.HomeSwitch). | |||||||||
Axisxx.HomeInputSelect | SINT | Determines the corresponding input point to use as the Home Limit
Switch trigger. You cannot associate the same local input to multiple axes or axis
functions. |
| |||||||||
Axisxx.PositiveOvertravelInputSelect | SINT | Determines the input point to use as the positive overtravel
trigger. You cannot associate the same local input to multiple axes or axis
functions. |
| |||||||||
Axisxx.NegativeOvertravelInputSelect | SINT | Determines the input point to use as the negative overtravel
trigger. You cannot associate the same local input to multiple axes or axis
functions. |
| |||||||||
Axisxx.HomeTimeout | DINT | Specifies the maximum time that the axis is allowed to find the home
position. When the time elapses, the axis performs a smooth stop and the
position stays invalid. | 1000…600,000 ms | |||||||||
Axisxx.HomeSpeed | REAL | Specifies the speed to use during a Home operation until the home
limit switch is detected. You can set this parameter to a high value
to reduce the time it takes to perform the Home command. The value is in Engineering Units per second. | Any positive value | |||||||||
Axisxx.HomeFinalSpeed | REAL | Specifies the final speed to use after the home limit switch is
detected. You can set this parameter to a low value to achieve
better home position accuracy. The value is in Engineering Units per second. | Any positive value | |||||||||
Axisxx.HomeAccel | REAL | Specifies the speed's rate of change for the Home command. The value is in Engineering Units per second 2 . | Any value | |||||||||
Axisxx.BrakeDisengageDelayTime | INT | Specifies the delay time, in milliseconds, from axis power turned on
until the brake is released. | 0…1000 ms | |||||||||
Axisxx.BrakeEngageDelayTime | INT | Specifies the delay time, in milliseconds, from axis power turned off
until the brake is applied. | 0…1000 ms | |||||||||
Inputxx.InputOffOnFilter | SNT | The amount of time that a signal must be in the On state before the
input data indicates the On state. The amount of time is indicated using an enumeration. |
| |||||||||
Inputxx.InputOnOffFilter | SINT | The amount of time that a signal must be in the Off state before the
input data indicates the Off state. The amount of time is indicated using an enumeration. |
|
Provide Feedback