AxisXX – Brake view parameters

The
AxisXX – Brake
view includes these parameters:
Parameter
Description
Disengage Delay Time
Specifies the delay time from axis power turned on until the brake is released.
Valid values are 0…1000 ms
Engage Delay Time
Specifies the delay time from axis power turned off until the brake is applied.
Valid values are 0…1000 ms
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal