Downloads
What does this application do?
The PlantPAx System Status (SysSts) feature was developed to provide a centralized view of the operational health of the automation system. It continuously monitors controllers, operator stations, servers, networks, and critical system services, identifying failures, loss of communication, offline equipment, and abnormal conditions before they impact operation.
- General Characteristics
- Advantages
- Limitations and Disadvantages
PlantPAx System Status (SysSts) is an integrated diagnostic tool that provides a consolidated view of the operational health of the control system. The solution continuously monitors controllers, servers, operator stations, communication networks, and critical services, graphically and consistently presenting the operational conditions of the architecture. Through visual indicators and centralized diagnostics, it makes it possible to quickly identify failures, loss of communication, and abnormal conditions that may impact system performance.
- Significant reduction in diagnostic time.
- Proactive detection of problems before they affect production.
- Greater system availability.
- Easier maintenance and support.
- Less dependence on specific knowledge of each piece of equipment.
- Single view of the health of the entire architecture.
- Acceleration of commissioning and startup activities.
- Better experience for operators and maintenance teams.
- Requires the equipment to be correctly configured and integrated into PlantPAx.
- The quality of the information depends on the correct configuration of the architecture.
- Does not replace specialized network or server diagnostic tools.
- May require training for full interpretation of the diagnostics presented.
- Legacy systems may require adaptations to provide all status information.
Please note: You will need to agree to the Terms & Conditions for each download.
Need Help?
If you need help with an application or have feedback from the Innovation Center, please contact us.
Is this application relevant to me?
This functionality is extremely advantageous for users seeking greater operational availability and reduced plant downtime. By providing a centralized view of the condition of the entire PlantPAx system, the tool simplifies maintenance and troubleshooting activities, making it possible to quickly identify the source of failures and act more efficiently. As a result, the time spent searching for the root cause of problems is reduced, system reliability is increased, and the productivity of operation and maintenance teams is improved.
How can I make it work?
Requirements: products, tools, prior knowledge.
Hardware
- Compatible ControlLogix or CompactLogix controllers.
- PlantPAx server.
- Operator Stations (Operator Workstations).
- EtherNet/IP infrastructure.
Software
- FactoryTalk View SE.
- PlantPAx Library.
- FactoryTalk Linx.
- Studio 5000.
- Standard PlantPAx diagnostic objects and displays.
Prior Knowledge
- As a prerequisite, it is recommended that everyone involved has prior knowledge of the subject and hold the PlantPAx Badge, available in the Partner Program.
Note: Read the PDF "PlantPAx Capability Overview 1" available in the Downloads.
Implementation Guide
- Step 1.1
- Step 1.2
- Step 1.3
- Step 1.4
- Step 1.5
- Step 1.6
- Step 1.7
- Step 1.8
- Step 1.9
- Step 1.10
- Step 2.1
- Step 2.2
- Step 2.3
- Step 2.4
Download the standard application.
Install Common Application Libraries.
Video 01_ ACM_CommApplicationLibraries
Install Libraries.
Video 02_ ACM_Install Libs
Install the Process Library from Application Code Manager.
Video 03_ Install Process Lib ACM
Install Studio5000 with Version 37.
Video 04_ Studio5000_Install_V37
Install FactoryTalk View.
NOTE: Studio Enterprise is used. Directory Type created as Standard. TLS disabled.
Video 05_ FTView_Install
Install Patch.
NOTE: Patch cannot be in .zip format.
Video 06_ Install Patch
Restore APB Reference Application
NOTE: Use the README.txt file for the PlantPAx Password.
Video 07_ Restore APB Application
Open Application After APB Restore.
Video 08_ Opening Application after APB restore
Configure Frame to obtain Preconfigured CLI.
Video 09_ Configuring the Frame_CLI_Preconfigured
Install FactoryTalk Echo.
Video 10_ FTEcho_installation
Loading configurations according to Rockwell manuals.
Follow the operating instructions in the video.
IMPLEM_1
Access the FactoryTalk System Status Portal.
implementing-plantpax-system-status-and-diagnostics-benefits_step3.1.png
Access the Reference Application: PlantPAx_v5_50.
implementing-plantpax-system-status-and-diagnostics-benefits_step3.2.1.png
implementing-plantpax-system-status-and-diagnostics-benefits_step3.2.2.png
Explore the Application.
Example Screen available with System Status and Diagnostics.
implementing-plantpax-system-status-and-diagnostics-benefits_step3.3.png
Implementing PlantPAx System Status and Diagnostics Benefits
Version 1.0 - October 2026