Clear a Fault

IMPORTANT: Before you clear major faults, export the system history.
Faults can be cleared automatically or manually, depending on the severity:
  • A major or minor recoverable fault is automatically cleared when the cause of the fault is resolved. If the fault is raised and immediately resolved by firmware, the fault persists for at least 1 minute.
  • A major nonrecoverable fault is cleared manually by one of these methods:
    • Restart the module. - Remove and insert the module in the chassis while power is applied.
    • Select the Clear Fault button below the fault log in the RMCT. With this feature, you can remotely restart a redundancy module without physically removing and reinserting it in the chassis. The Clear Fault button is active only when the redundancy module is in a major fault state.
Clear a Major Nonrecoverable Fault
Clear Fault button in RMCT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal