Fiber Channel Operation

The dual SFP ports on the redundancy module operate as a redundant communication channels between partner redundancy modules. On 1756-RM3 modules, communication occurs on both channels. If one channel fails, communication persists on the other channel with no delay. Channel switchovers do not occur on 1756-RM3 modules.
IMPORTANT:
When you connect the fiber channels between partner redundancy modules, connect matching ports. For example, connect Link 1 on the primary module to Link 1 on the secondary module.
The use of both fiber channels is not required, but recommended for redundancy.

Causes of a Fiber Channel Failure

Any of the following can cause a loss of operation between fiber channels:
  • Signal attenuation along the fiber cable path that is routed between the partner redundancy modules
  • A broken or damaged fiber cable that is routed between the partner redundancy modules
  • Improper or loosely fit cable connector
  • SFP transceiver fault
  • Removal or loose connection of the SFP transceiver
  • Data communication error that is signaled by a failed CRC check

Identify Installed SFP Transceivers

You can identify the SFP transceivers that are installed in the dual SFP ports from the Module Info tab in the
FactoryTalk® Linx
Redundancy Module Configuration Tool (RMCT). The SFP Type Link 1 and SFP Type Link 2 fields display one of the following values:
  • SFP Not Present
  • SFP Not Supported
  • 1783-SFP1GSX
  • 1783-SFP1GLX
  • 1783-SFP1GEXE
  • 1783-SFP1GZX
For SFP transceiver technical specifications, see the ControlLogix and GuardLogix Controller Specifications Technical Data, publication 1756-TD001.
SFP Transceiver Identification
SFP Type Link 1 and SFP Type Link 2 fields on the Module Info tab
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal