Enter Redundancy Module Identification Information

You can enter general identification information about the redundancy module that is connected to the
FactoryTalk® Linx
Redundancy Module Configuration Tool (RMCT):
  • Identification information is not crossloaded to the partner redundancy module.
  • Identification information is maintained in nonvolatile memory, so that the chassis identity is retained through power cycles.
By default, identification parameters are empty.
Module Identification
1756-RM3 User-Defined Identity Dialog Box
To enter identification information for a redundancy module, follow these steps.
  1. Access the RMCT.
  2. Select the Module Info tab.
  3. In the User-Defined Identity area, select Change.
  4. Enter the identification information and select OK.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal