Troubleshoot the Controller
There are many options available to troubleshoot the controller if issues occur during normal operation.
You can use the
Studio 5000 Logix Designer®
application to view fault conditions in these ways:- Module status in the I/O Configuration Tree
- Categories on I/O Module Properties Dialog
- Notification in the Tag Monitor
- Fault Information in the Controller Properties Dialog
- Ethernet Port Diagnostics
- Advanced Time Sync dialog
You can also use:
- Diagnostic information in Linx-based software
- Controller Webpages
Provide Feedback