Nodes on an EtherNet/IP Network

When configuring your control system, you must account for the number of
EtherNet/IP
nodes you include in the I/O configuration tree in your project.
Maximum Number of Ethernet Nodes
This image shows where information on the number of Ethernet Nodes is in Logix Designer.

Devices Included in the Node Count

Any
EtherNet/IP
devices that you add to the I/O configuration section are counted toward the controller node limits. The following are examples of devices that must be counted:
  • Remote communication adapters
  • Remote controllers
  • Devices with an embedded EtherNet/IP port
  • EtherNet/IP
    devices that are added to the I/O tree under a communication module in the local chassis, even though the communication module in the local chassis does not count as a node
  • HMI devices that are added to the I/O tree
  • Third-party devices that are directly connected to the
    EtherNet/IP
    network

Devices Excluded from the Node Count

When considering the
EtherNet/IP
node limitation of a controller, you do not count Ethernet devices that exist on the
EtherNet/IP
network but are not added to the I/O configuration section of the project.
The following devices are not added to the I/O configuration section in your project and are not counted among the total number of nodes:
  • Computer
  • Communication modules in the local chassis
  • HMIs that are not added to the I/O configuration section
  • Devices that are the target of MSG Instructions
  • Standard Ethernet devices with which the controller communicates via a socket interface
The following example shows five nodes in the I/O tree.
Ethernet Nodes Example
This image shows nodes in the I/O configuration in Logix Designer.
Item Description
Item
Description
A
Not a node. Module is in the local chassis.
B
Node
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal