Summary of Changes
    The following is new or updated information. This list includes substantive updates only and is not intended to reflect all changes. Translated versions are not always available for each revision.
Topic  | Page  | 
|---|---|
Added hardware fault tolerance requirements for high-demand applications  | |
Safety signatures can be generated in Remote Run mode  | 
Provide Feedback