Failed to delete rung # <Rung Number>
Tried to delete a rung in the routine, but the operation did not succeed. This could occur because:
- the routine was deleted
- the rung number is invalid
- the rung was not a valid type that can be deleted
- there is insufficient memory
Provide Feedback