Use the Filters check boxes
Use the
Module Type Category Filters
and Module Type Vendor Filters
check
boxes to locate a specific module type. This example is based on searching for a 1756
diagnostic input module that is manufactured by Allen-Bradley but not knowing the actual
catalog number, which is 1756-IA8D. Use the check boxes in the Module Type Category
Filters
box and the Module Type Vendor Filters
box to narrow the list of
modules.To use the filters check boxes
- In theSelect Module typedialog box,Catalogtab, in theModule Type Category Filterslist, clear theCommunicationandControllercheck boxes, knowing that the 1756-IA8D module is not in one of these categories.
- Leave all the check boxes selected in theModule Type Vendors Filterslist.

- Right-click the1756-IA8Dmodule in the Catalog Results list and selectCreate.TIP: Another option is to select the module and then selectCreate.
Provide Feedback