Locate target modules using the Catalog tab
Use the Search box or a combination of filters to locate a specific module type. This example for locating module types is based on searching for a 1756 diagnostic input module that is manufactured by Rockwell Automation/Allen-Bradley but not knowing the actual catalog number, which is 1756-IA8D.
To locate target modules using the Catalog tab
Start typing the word
diagnostic
into the Search box:- In theSelect Module typedialog box,Catalogtab Search box, type the letterd.Note that there are no changes in the list of displayed module types since virtually everything contains the letter d.
- Add the lettersiagto the d.The Search box now contains the letters diag. The Catalog Results list displays all results where either theCatalog Numberor theDescriptionor theVendorhas the letters diag, as shown below.

- Right-click the1756-IA8Dmodule that is part of the Catalog Results list and selectCreate.
Provide Feedback