System protocol for sending broadcast messages

The Broadcast button is enabled when you choose one of the following protocols in the
Controller Properties dialog box - System Protocol
tab.
NOTE: Logix Designer versions 37 and later do not support controllers with serial ports. The
Broadcast
button and the
System Protocol
tab appear only in Logix Designer versions 36 and earlier for controllers with a serial port.
  • DF1 Master
  • DF1 Radio Modem
  • DF1 Slave
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal