Updated instruction mnemonics

In Logix Designer versions 36 and later, these instruction mnemonics have been updated to conform to IEC 61131-3 and PLCopen standards.
Instruction
Mnemonic in versions v35 and earlier
Mnemonic in versions v36 and later
Arc Cosine
ACS
Arc Sine
ASN
Arc Tangent
ATN
Convert to BCD
TOD
Convert to Integer
FRD
Equal To
EQU
Greater Than
GRT
Greater Than or Equal To
GEQ
Less Than or Equal To
LEQ
Less Than
LES
Limit
LIM
Move
MOV
Not Equal To
NEQ
Square Root
SQR
Truncate
TRN
X to the Power of Y
XPY
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal