Specify Bits Within Arrays

You can address bits within elements of arrays. For example:
Definition
Example
Description
array1
defined as DINT[5]
array1[1].2
This example references the bit 2 in element 1 of the array.
array2
defined as INT[17,36]
1
st
dimension has 17 elements
2
nd
dimension has 36 elements
array2[3,4].15
This example references the bit 15 of the element array2[3,4].
array3
defined as SINT[2,4,6]
1
st
dimension holds 2 elements
2
nd
dimension holds 4 elements
3
rd
dimension holds 6 elements
array3[1,3,2].4
This example references bit 4 of the element array3[1,3,2].
MyArray defined as SINT[100]
MyIndex defined as SINT
MyArray[(MyIndex AND NOT 7) / 8].[MyIndex AND 7]
This example references a bit within a SINT array.
MyArray defined as INT[100]
MyIndex defined as INT
MyArray[(MyIndex AND NOT 15) / 16].[MyIndex AND 15]
This example references a bit within an INT array.
MyArray defined as DINT[100]
MyIndex defined as DINT
MyArray[(MyIndex AND NOT 31) / 32].[MyIndex AND 31]
This example references a bit within a DINT array.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal