Controlling a Ratio (PID)

You can maintain two values in a ratio by using these parameters:
  • Uncontrolled value
  • Controlled value (the resultant setpoint to be used by the PID instruction)
  • Ratio between these two values
Ladder Diagram
TIP: To avoid locking up the PID with invalid internal floating point values, ensure the PV is not INF or NAN before invoking the instruction such as:
  • XIC (PC_timer.DN)
  • MOV(Local:0:1.Ch0Data, Local:0:1.Ch0Data)
  • XIO(S:V)
  • PID(...)
Structured Text
pid_2.sp := uncontrolled_flow * ratio
PID(pid_2,pv_2,tieback_2,cv_2,0,0,0);
TIP: To avoid locking up the PID with invalid internal floating point values, ensure the PV is not INF or NAN before invoking the instruction such as:
  • XIC (PC_timer.DN)
  • MOV(Local:0:1.Ch0Data, Local:0:1.Ch0Data)
  • XIO(S:V)
  • PID(...)
For this multiplication
Enter this value
Destination
Controlled value
Source A
Uncontrolled value
Source B
Ratio
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal