MVC wiring and programming example

This topic demonstrates how to wire the Guard I/O module and program the instruction in the safety control portion of an application.
TIP: The standard control portion of the application is not shown in the following diagram.
Wiring Diagram
MVC Wiring and Programming Example
This programming diagram shows the Main Valve Control (MVC) instruction with inputs and outputs.
Programming Diagram
MVC Programming Example
Ladder Diagram
RSL5K_MVC_exampleladder_v31
Module Definition
The following sections provide examples of how to use the programming software to set the Guard I/O module configuration operands.
RSL5K_Module Definition for Safety and Metal Instructions_v31
Rockwell Automation suggests selecting
Exact Match
for the
Electronic Keying
as shown. It also acceptable to select
Compatible Match
.
Module Input Configuration
RSL5K_MVC_InputConfig_v31
Module Test Output Configuration
RSL5K_MVC_TestOutputConfig_v31
Module Output Configuration
RSL5K_MVC_OutputConfig_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal