Specify SLC Messages

Use the SLC message types to communicate with SLC and MicroLogix controllers. The following table specifies which data types the instruction allows you access. The table also shows the corresponding
Logix 5000
data type.
For this SLC or MicroLogix data type:
Use this
Logix 5000
data type:
F
REAL
L (MicroLogix 1200 and 1500 controllers)
DINT
N
INT
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal