Equipment Phase Instructions

The Equipment Phase instructions include:
Available Instructions
Ladder Diagram and Structured Text
Function Block
These instructions are not available in function block.
If want to:
Use this instruction:
Signal an equipment phase that the state routine is complete to indicate that it should go to the next state
PSC
Change the state or substate of an equipment phase
PCMD
Give a Hold, Stop, or Abort command to an equipment phase, regardless of ownership
POVR
Signal a failure for an equipment phase
PFL
Clear the failure code of an equipment phase
PCLF
Initiate communication with FactoryTalk Batch software.
PXRQ
Clear the NewInputParameters bit of an equipment phase
PRNP
Set up breakpoints within the logic of an equipment phase
PPD
Take ownership of an equipment phase to either:
  • Prevent another program or FactoryTalk Batch software from commanding an equipment phase
  • Make sure another program or FactoryTalk Batch software does not already own an equipment phase
PATT
Relinquish ownership of an equipment phase
PDET
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal