Motor Test Result Attributes

These are the attributes that are associated with result status applied to a Motion Control Axis.
Motor Test Status
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
Get/GSV
USINT
-
-
-
Enumeration:
0 = test process successful
1 = test in progress
2 = test process aborted
3 = test process timed-out
4 = test process faulted
5 = test reached travel limit
6 = reserved
7 = test measurement error
8 = test configuration error
9-127 = reserved
128-255 = vendor specific
128= test prohibited - axis test mode active
The Motor Test Status attribute returns status of the last Run Motor Test service on the targeted drive axis. The Motor Test Status attribute can be used to determine when the motor test service has successfully completed. Conditions may occur, however, that make it impossible for the drive to properly perform the operation. When this is the case, the test process is automatically terminated and a test error is reported that is stored in the Motor Test Status output parameter. Values in the normal vendor specific range (128-255) correspond to values defined in the vendor-specific range in the open service on the device.
Motor Test Resistance
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
Get/GSV
REAL
-
-
-
Ohms
This floating point value represents the stator resistance of an induction or permanent magnet motor as measured by the Motor Test procedure.
Motor Test Inductance
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IM, SPM only
Get/GSV
REAL
-
-
-
Henries
This floating point value represents the motor inductance of an induction or permanent magnet motor as measured by the Motor Test procedure.
Motor Test Flux Current
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IM Only
Get/GSV
REAL
-
-
-
Amps
This floating point value represents the motor flux current of an induction motor as measured by the Motor Test procedure.
Motor Test Slip Speed
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IM Only
Get/GSV
REAL
-
-
-
RPM: rotary motor type
m/s: linear motor type
This floating point value represents the slip speed of an induction motor as measured by the Motor Test procedure.
Motor Test Counter EMF
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
PM Only
Get/GSV
REAL
-
-
-
Volts
This floating point value represents the measured Counter EMF (CEMF) of a PM motor at Rated Speed by the Motor Test procedure.
Motor Test Lq Inductance
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IPM Only
Get/GSV
REAL
-
-
-
Henries
This floating point value represents the phase-to-phase q-axis motor inductance measured by the Motor Test procedure.
Motor Test Ld Inductance
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IPM Only
Get/GSV
REAL
-
-
-
Henries
This floating point value represents the phase-to-phase d-axis motor inductance measured by the Motor Test procedure.
Motor Test Lq Flux Saturation
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IPM Only
Get/GSV
REAL [8]
-
-
-
% Nominal Inductance
This floating point value represents the phase-to-phase q-axis stator inductance of the motor as measured by the Motor Test procedure expressed as a percentage of the measured Nominal Inductance, Lq, at 25%, 50%, 75%, 100%, 125%, 150%, 175% and 200% rated continuous current.
Motor Test Ld Flux Saturation
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IPM Only
Get/GSV
REAL
-
-
-
% Nominal Inductance
This floating point value represents the phase-to-phase d-axis stator inductance of the motor as measured by the Motor Test procedure expressed as a percentage of the measured Nominal Inductance, Ld, at 100% rated continuous current.
Motor Test Bus Overvoltage Speed
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IPM Only
Get/GSV
REAL
-
-
-
RPM (rotary motor type)
m/s (linear motor type)
This floating point value represents the maximum speed of the motor without exceeding the operational DC bus overvoltage limit, as determined by the Motor Test procedure.
Motor Test Commutation Offset Comp
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
IPM Only
Get/GSV
REAL
-
-
-
Electrical Degrees
This floating point value represents the change in motor Commutation Offset at rated continuous current as measured by the Motor Test procedure.
Motor Test Flux Saturation
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - D
SPM Only
Get/GSV
REAL[8]
-
-
-
% Nominal Inductance
Array of measured phase-to-phase stator inductance of the motor as a percentage of the measured Nominal Inductance, PM Motor Inductance, at 12.5%, 25%, 37.5%, 50%, 62.5%, 75%, 87.5% and 100% of the Peak Current Rating.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal