Rockwell Automation Specific Initialization Faults

This table defines a list of Rockwell Automation specific faults associated with the Initialization Faults-RA attribute.
Rockwell Automation Specific Initialization Faults Bit Descriptions
Bit
Fault
Description
0
Reserved
This bit cannot be used since the Fault Code is defined by the associated exception bit number and Fault Code of 0 means no fault condition is present.
1
Feedback Data Corruption
Smart Encoder Data Corruption detected.
2
Feedback Data Range
Data within a motor data blob is out of range.
3
Feedback Communication Startup
Communications with a smart encoder could not be established.
4
Feedback Absolute Overspeed
Excessive speed was detected in the battery-backed encoder while power was off.
5
Feedback Absolute Power Off Travel
The power-off travel range of the battery-backed encoder has been exceeded.
6
Feedback Absolute Startup Speed
The absolute encoder was not able to accurately determine the position after power-up due to speed greater than 100 RPM.
7
Commutation Offset Uninitialized
The commutation offset stored in a third-party motor has not been initialized.
8
Reserved
-
9
Reserved
-
10
Reserved
-
11
Reserved
-
12
Invalid FPGA Image
The FPGA image is incompatible with hardware operation.
13
Invalid Board Support Package
The board support package is incompatible with hardware operation.
14
Invalid Safety Firmware
The safety firmware is not compatible with the drive firmware, or the main safety firmware is missing.
15
Power Board
Power Board checksum error.
16
Illegal Option Card
The Main Control Board has detected an illegal option installed in the port.
17
Option Storage Checksum
Option data storage checksum failed.
18
Reserved
-
19
Module Voltage Mismatch
Voltage rating mismatch detected on the inter-device communications backplane.
20
Unknown Module
Unknown device detected on the inter-device communications backplane.
21
Factory Configuration Error
Factory Configuration Data is missing or invalid.
22
Illegal Address
Invalid Ethernet IP Address configuration or device Node Address is out of range (>254).
23
Series Mismatch
Incompatible device is detected on the inter-device communications backplane, for example, SERCOS AMs have been detected by the CIP IAM.
Rockwell Automation
24
Open Slot
Open slot detected on the inter-device communications backplane.
25
Mover Axis Assignment
Track section has detected a mover to axis assignment error.
26
Track Backplane Communication
Track section has detected a problem initializing the section addresses required to support backplane communication around the track.
27
Unassociated Section Axis
Track section has detected that section axis instance data is missing from the connection and the section axis has not been configured. This condition occurs when the section axis instance has not been associated with an axis instance of the controller, or if the section axis has been inhibited. All mover axes associated with this section module shall assert this fault.
28
Track Configuration
Track system has encountered a configuration error with one of track sections that prevented the track from performing the mover axis assignment function. The section number of the erred track section is passed in the Sub Code.
29-31
Reserved
-
Rockwell Automation CIP Initialization Fault Name Mapping
Bit
Object CIP Initialization Fault Name
0
-
1
Feedback Data Corruption Fault
2
Feedback Data Range Fault
3
Feedback Communication Startup Fault
4
Feedback Absolute Overspeed Fault
5
Feedback Absolute Power Off Travel Fault
6
Feedback Absolute Startup Speed Fault Fault
7
Commutation Offset Uninitialized
8
-
9
-
10
-
11
-
12
Invalid FPGA Image Fault
13
Invalid Board Support Package Fault
14
Invalid Safety Firmware Fault
15
Power Board Fault
16
Illegal Option Card Fault
17
Option Storage Checksum Fault
18
-
19
Module Voltage Mismatch
20
Unknown Module Fault
21
Factory Configuration Error Fault
22
Illegal Address Fault
23
Series Mismatch Fault
24
Open Slot Fault
25
Mover Axis Assignment Fault
26
Track Backplane Communication Fault
27
Unassociated Section Axis Fault
28
Track Configuration Fault
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal