Communication Formats: Non-I/O Modules
The modules and corresponding communication formats are listed in the tables below.
TIP:
The default communication formats are shown in bold.
The Communication Format you choose for ControlNet Adapters allows rack-based communication to occur with digital I/O modules in the same chassis as the adapter.
Refer to the Logix 5000 Controllers Common Procedures manual (publication 1756-PM001) for
more detailed information on choosing the appropriate Comm Format.
For these modules: | These communication formats are available: |
1734-ACNR/A 1734-AENT/A 1738-ACNR/A 1738-AENT/A 1756-CNB/A 1756-CNB/B 1756-CNB/D 1756-CNBR/A 1756-CNBR/B 1756-CNBR/D 1756-ENBT/A 1756-ENBT/B 1756-ENET/B | Listen Only - Rack Optimization None
TIP:
For the 1756 Ethernet adapters, there is no
default Comm Format, however these 3 formats are available.
|
CONTROLNET-MODULE ETHERNET-MODULE | Data - DINT Data - DINT-With Status Data - INT Data - INT-With Status Data - REAL Data - REAL-With Status Data - SINT Data - SINT-With Status Input Data - DINT Input Data - DINT-Run/Program Input Data - DINT-With Status Input Data - INT Input Data - INT-Run/Program Input Data - INT-With Status Input Data - REAL Input Data - REAL-With Status Input Data - SINT Input Data - SINT-Run/Program Input Data - SINT-With Status |
1771-ACN15 1771-ACNR15 | Listen Only - Rack Optimization Rack Optimization |
1788-CN2DN 1788-EN2DN/A | Data Input Data |
1794-ACN15/C 1794-ACNR15/C | None (i.e., Rack communications is not possible) Rack Optimization
TIP:
There is no Listen Only Rack Optimization
option for Flex.
|
1794-AENT/A 1794-AENT/B 1797-ACNR15 | None (i.e., Rack communications is not possible) Rack Optimization |
ETHERNET-PanelView | Data - INT Input Data - INT Data - DINT Input Data - DINT |
The Communication Format you choose for a 2711 PanelView Operator Terminal determines the
size of the Input and Output Data sizes (32 Integer and 8 Integer sizes are available).
For this module: | These communication formats are available: |
2711 PanelView Operator Terminal | Data - 32 INT
Data - 8 INT |
The Communication Format you choose for a 56AMXN DCSNet Interface determines the corresponding connection count.
For this module: | These communication formats are available: | With these data connection counts: |
56AMXN DCSNet Interface | Master - 7 Drops | 2 |
Master - 14 Drops | 3 | |
Master - 21 Drops | 4 | |
Master - 28 Drops | 5 | |
Master - 35 Drops | 6 | |
Master - 42 Drops | 7 | |
Master - 49 Drops | 8 | |
Master - 56 Drops | 9 | |
Master - Listen Only - 7 Drops | 2 | |
Master - Listen Only - 14 Drops | 3 | |
Master - Listen Only - 21 Drops | 4 | |
Master - Listen Only - 28 Drops | 5 | |
Master - Listen Only - 35 Drops | 6 | |
Master - Listen Only - 42 Drops | 7 | |
Master - Listen Only - 49 Drops | 8 | |
Master - Listen Only - 56 Drops | 9 | |
Slave - 7 Drops | 2 | |
Slave - 14 Drops | 3 | |
Slave - 21 Drops | 4 | |
Slave - 28 Drops | 5 | |
Slave - 35 Drops | 6 | |
Slave - 42 Drops | 7 | |
Slave - 49 Drops | 8 | |
Slave - 56 Drops | 9 | |
Slave - Listen Only - 7 Drops | 2 | |
Slave - Listen Only - 14 Drops | 3 | |
Slave - Listen Only - 21 Drops | 4 | |
Slave - Listen Only - 28 Drops | 5 | |
Slave - Listen Only - 35 Drops | 6 | |
Slave - Listen Only - 42 Drops | 7 | |
Slave - Listen Only - 49 Drops | 8 | |
Slave - Listen Only - 56 Drops | 9 |
Provide Feedback