DANGER. Disabling Automatic Output Processing prevents outputs from being sent automatically to the I/O module
When you choose to disable automatic output processing to reduce task overhead, outputs are not sent automatically to the I/O module.
Either enable automatic output processing on at least one frequently executed task or use the Immediate Output Instructions (IOT) in the application logic to make sure all of the outputs are sent on a regular basis.
Provide Feedback