Add a subdevice
You can add a new subdevice or duplicate an existing subdevice.
Add a new subdevice
- In the, access the section.FactoryTalk® Remote Access™Manager
- In the domain left pane, select the primary device on which the subdevice is dependant.
- Next to the primary device, in its same line, select
. Alternatively,
select the three dots at the top of the screen and select Add subdevice. - ACreate subdevicedialog window opens. Enter the subdeviceNameandIP address.NOTE: The subdevice IP address must be compatible with a subnet that is reachable by the remote device.
- SelectSave.
Duplicate an existing subdevice
You can duplicate subdevices from one device to another while preserving their
configuration and associated services, eliminating the need for manual redefinition and
reducing setup time.
- InDomain view, right-click the subdevice you want to duplicate.
- SelectCopy subdevice.TIP: To duplicate all subdevices under a device, right-click the device and selectCopy subdevices.
- Select the destination device.
- SelectPaste subdevice, orPaste subdevicesif you previously selectedCopy subdevices.The duplicated subdevice(s) will appear in the left pane, under the selected device.
IMPORTANT:
You cannot duplicate one or more subdevices
within the same device.
IMPORTANT:
Duplication is not possible if the destination device already contains
one or more subdevices with conflicting IP addresses.
Provide Feedback