Sizing Architecture Examples
Runtime entitlements are based on the number of feature tokens that your application
requires. The examples that are given in this section are typical applications; your own
architecture can be different than what is shown.
Package sizes:
- XS - extra small; up to five tokens
- S - small; up to eight tokens
- M - medium; up to 11 tokens
- L - large; up to 15 tokens
- XL - extra large; up to 21 tokens
Provide Feedback