Getting Started with FactoryTalk Hub
FactoryTalk Hub is the online location where you can access Rockwell
Automation's cloud-based Software as a Service (SaaS) offerings to simplify the way you
design, create, and maintain your assets.
To get started with FactoryTalk Hub, you must:
- Browse to and sign in to FactoryTalk Hub.
- Join or create a FactoryTalk Hub organization. See Join an Organization or Create an Organization.
NOTE:
The
organization
you belong to controls the services available to you in
FactoryTalk Hub.Authentication
FactoryTalk Hub uses your MyRockwell user
profile
to authenticate your access and determine your organization.
You can be a member of more than one organization.When you authenticate and you log on to FactoryTalk Hub, your browser displays the
Organizations
page if you are a new user. Existing user go to their
Applications
page.If you are a new user, you see options to create or join an organization. If you are already
a member of one or more organizations, you see a list of organizations you are assigned
to.
Once you select an organization, in the top left corner you see the breadcrumb showing the
organization you will be working on.
TIP:
The
breadcrumb only changes when you select a different organization to show which organization
you are currently working with.
IMPORTANT:
Upon the first use of some
FactoryTalk®
Hub™
applications, you are prompted for multifactor
authentication. You must have an authenticator app, such as Microsoft®
Authenticator.Provide Feedback