Configure runtime as a service
Install and configure FactoryTalk Optix Runtime Tools to launch
FactoryTalk Optix Applications
in the runtime-as-a-service
mode.- During the FactoryTalk Optix Runtime Tools installation:
- SelectCustomize.
- ExpandFactoryTalk Optix Runtime Tools,VERSIONwhereVERSIONis the FactoryTalk Optix Runtime Tools version.
- SelectRun FactoryTalk Optix as a Service.
TIP: To change the runtime mode between the default runtime-application mode and runtime-as-a-service mode, you need to reinstall FactoryTalk Optix Runtime Tools.For more information, see Install Runtime Tools on Windows devices. - Deploy the application to the target device in the runtime-as-a-service mode.For more information, see Deploy a FactoryTalk Optix application.
Provide Feedback