Time zones
Overview of supported time zones and event properties for date and time
management, including alarm events and trend graphs.
Supported time zones
FactoryTalk Optix
supports three time zones:- UTC standard time zone.
- Local time zone of the machine running theFTOptixApplication.
- Session time zone supported by applications in remote sessions.
Date and time event properties
The date and time format follows the specifications of the OPC UA data type
DateTime
.The
BaseEventType
object properties that manage date and time
events include:Property | Data type | Description |
|---|---|---|
Time | UtcTime | Date and time of the UTC standard time zone + 0. |
LocalTime | TimeZoneDataType | Offset in minutes between the UTC date and time and the local
date and time of the device for the application. For example, on a
device set to UTC + 2, the offset is 120 minutes. If applicable, the
offset may include DaylightSavingInOffset . |
TimeZoneOffset | TimeZoneDataType | Session offset of UTC + 0 for the date and time. |
Time zones for alarm events
At runtime, the
Data grid
object of the Alarm
grid
and Alarm log grid
objects display the
local time of events in the Timestamp
column.Object | Timestamp |
|---|---|
Alarm grid | Set a dynamic link in the Time
property. |
Alarm history grid | Set a dynamic link in the Time property
with a node pointer. |
In projects that support remote sessions, devices with different local time settings
can display different time zones in the widgets. The timestamp of the widget
displays in the local time zone of the device, even when events occur in different
time zones. In the
Timestamp
column of the Alarm
grid
or Alarm history grid
, set a converter
of type Expression evaluator
with the sum of the properties
{Item}Time
and
{Session}TimeZoneOffset
.Time zones in trends
At runtime, the
Trend
object displays data in the X-axis in
the UTC standard time zone.Use the
Reference time zone
property of the graph to specify
if data displays in the local time zone or the session time zone. If the
Trend
object connects to a Data
logger
, enable the Local time log
property of
the application to store data in the local time zone.Time zone
UTC
Local time
Session time zone
Alarm events
Trend graphs
Provide Feedback