Change UI scaling
Adjust the scale factor for UI elements to modify their size in the application
interface.
- InProject viewselect the applicableUISessionobject.
- InPropertiesedit theScale factorvalue.The default size of the UI elements is multiplied by the scale factor. For example, if you set the factor to2, all UI objects and fonts will be twice larger than their local size value.TIP: You can also create dynamic links through the{Session}/ScaleFactoralias to control the scale dynamically for graphic objects. You can create the dynamic link even without a custom UISession object in the presentation engine.The scale factor you set is retained after you close and reopen the application, and persists until modified again.
Provide Feedback