UploadFileCompletedEvent

Event argument details and data types for UploadFileCompletedEvent, including variable descriptions and result codes.

Event arguments

You can use the following variables exposed by this alias in your application logic:
{Session}
Session
UI Session
UISession
#
UploadFileCompletedEventHandler
#
EventArguments
.
For more information about aliases, see Aliases.
Event arguments
Variable
Data type
Description
Operation ID
Guid
Unique identifier for the upload operation. See Method: Upload file.
Result code
Enum
  • 0
    . Upload completed successfully.
  • 1
    . Upload failed due to invalid folder or insufficient permissions.
  • 2
    . Upload failed due to file size exceeding the allowed limit.
  • 3
    . Upload failed due to unsupported file type or policy violation.
  • 4
    . Upload failed due to an internal error.
File path
String
Path to the uploaded file. Empty if the upload fails.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal