DownloadFileStartedEvent

Event argument details and data types for DownloadFileStartedEvent, including variable descriptions and result codes.

Event arguments

You can use the following variables exposed by this alias in your application logic:
{Session}
Session
UI Session
UISession
#
DownloadFileStartedEventHandler
#
EventArguments
.
For more information about aliases, see Aliases.
Event arguments
Variable
Data type
Description
Operation ID
Guid
Unique identifier for the download operation. See Method: Download file.
Result
Enum
  • 0
    . Download started successfully.
  • 1
    . No active download operations.
  • 2
    . Invalid or not existing file path.
  • 3
    . Unexpected requested resource path.
  • 4
    . Invalid or malformed file name.
  • 5
    . Forbidden resource path
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal