Native presentation engine
Use the native presentation engine for typical HMI applications that run on
targets with an operator panel.
Overview
A project can contain only one native presentation engine.
When you run a project, an interactive session generates and authenticates with the
starting user. You can change the current user in an interactive session. Based on
the user and logic created, the interface may change dynamically in the same
session.
TIP:
To specify the user, see Global methods for Session or Session activity log and audit.
To configure a native presentation engine, see Configure a native presentation engine.
SVG
Provide Feedback