Project information

When you open your project in the
FactoryTalk® Optix Studio
editor, a displayed message provides you with the actual number of nodes of the project. The message also contains the path of the project following the nodes count. In the same way, if you open the project file that has the extension “.optix” in the editor, you can find the project statistics about the following items, at the bottom of the file:
  • TotalNodeCount
  • Objects
  • ObjectTypes
  • Variables
  • VariableTypes
  • DataTypes
  • Methods
  • References
  • ReferenceTypes
  • Files
These statistics provide you with brief information about the project complexity and size.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal