Non-exclusive level alarm

Monitors when the values of interest are reached for variables relating to physical quantities. Activates when the value of the monitored variable reaches one or more limits of interest. When several limits of interest are reached consecutively, the alarm signals all the limits reached.
BrowseName
NonExclusiveLevelAlarmController
SuperType
Non-exclusive limit alarm(NonExclusiveLimitAlarmController)

Properties

Name
BrowseName
DataType
Description
High-high limit
HighHighLimit
(Inherited from Limit alarm)
High limit
HighLimit
(Inherited from Limit alarm)
Low limit
LowLimit
(Inherited from Limit alarm)
Low-low limit
LowLowLimit
(Inherited from Limit alarm)
Enabled
Enabled
(Inherited from Alarm controller)
Active
Active
(Inherited from Alarm controller)
Auto acknowledge
AutoAcknowledge
(Inherited from Alarm controller)
Auto confirm
AutoConfirm
(Inherited from Alarm controller)
Input variable
InputValue
(Inherited from Alarm controller)
Message
Message
(Inherited from Alarm controller)
Severity
Severity
(Inherited from Alarm controller)
Last event
LastEvent
(Inherited from Alarm controller)

Events

NonExclusiveLevelAlarmType
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.