Create an alarm trigger
Create a switch that triggers the ConveyorChassisMalfunction alarm.
- Create a switch that triggers the alarm:
- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the switch, select , and enterTriggerConveyorChassisMalfunctionAlarm.
- InProperties, create a dynamic link betweenActiveand .For more information about dynamic links, see Create dynamic links.
- Create a trigger label:
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the label, select , and enterTriggerAlarmLabel.
- InProperties, setTexttoTrigger the conveyor chassis malfunction alarm:.
Provide Feedback