Trend

View the trend of the values of one or more variables read in real time and/or logged.
BrowseName
Trend
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Model
Model
Reference to the information model or database from which to obtain the data.
Query
Query
Standard SQL query to filter the data of interest. You can use it to filter data from a database and to filter data obtained from a node-based model. In case of a node-based model, the SELECT * FROM Model part is mandatory, followed by the WHERE clause with which to indicate the search conditions - for example: SELECT * FROM Model WHERE Speed > 40
Refresh time
RefreshTime
Sampling interval in milliseconds.
Key visible
LegendVisible
Show/hide the legend of the pens.
Reference time zone
ReferenceTimeZone
Time zone for displaying the date and time on the X axis. (UTC: time zone standard; Locale: time zone of the device from which the data is generated; Session: session time zone). To record the data displayed in local time zone, enable the Local Time Log property of the Data logger object.
Pens
Pens
Trend lines. Trend pen collection of objects.
Pen X axis
XAxis
The X axis for the trend pen, that shows the time being measured. Can be set to automatically scroll forward in time during runtime by setting the Follow property to True.
Pen Y axis
YAxis
The Y axis for the trend pen, that shows the value of the variable being measured. Use the default Y axis values or set the properties to define minimum and maximum values. Can be set to automatically scale at runtime to resize the trend graph according the the values being displayed.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Methods

Refresh
BrowseName
Refresh
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.