Motion curve
- BrowseName
- EasingCurveEnum
Values
Value | DisplayName | Description |
---|---|---|
0 | Linear | |
1 | Quadratic In | |
2 | Quadratic out | |
3 | Quadratic In-Out | |
4 | Quadratic Out-In | |
5 | Cubic In | |
6 | Cubic Out | |
7 | Cubic In-Out | |
8 | Cubic Out-In | |
9 | Quartic In | |
10 | Quartic Out | |
11 | Quartic In-Out | |
12 | Quartic Out-In | |
13 | Quintic In | |
14 | Quintic Out | |
15 | Quintic In-Out | |
16 | Quintic Out-In | |
17 | Sinusoidal In | |
18 | Sinusoidal Out | |
19 | Sinusoidal In-Out | |
20 | Sinusoidal Out-In | |
21 | Exponential In | |
22 | Exponential Out | |
23 | Exponential In-Out | |
24 | Exponential Out-In | |
25 | Circular In | |
26 | Circular Out | |
27 | Circular In-Out | |
28 | Circular Out-In | |
29 | Elastic In | |
30 | Elastic Out | |
31 | Elastic In-Out | |
32 | Elastic Out-In | |
33 | Back In | |
34 | Back Out | |
35 | Back In-Out | |
36 | Back Out-In | |
37 | Bounce In | |
38 | Bounce Out | |
39 | Bounce In-Out | |
40 | Bounce Out-In |
Provide Feedback