Wi-Fi configuration
Configure the Wi-Fi network interface.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Operating mode | Mode | Adapter = the interface functions as a network adapter; Access point = the interface functions as an access point. | |
Username | Username | (Only if Security mode = WPA2-Enterprise) Name of the user to connect to the network. | |
Enable access to LAN network | EnableAccessToLanNetwork | Enable/disable access to the LAN sub-network for connected devices. |
Provide Feedback