Network interface

Configure the WAN and LAN network interfaces.
BrowseName
NetworkInterface
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Interface name
InterfaceName
Network interface to configure Values permitted: LAN, WAN, or Wi-Fi.
DHCP activated
DhcpEnabled
Enable/disable automatic IP address assignment in DHCP mode.
IP address
IPAddress
Primary IP address.
DNS 1
DNS1
(WAN and Wi-Fi interfaces only) DNS1 IP address
DNS 2
DNS2
(WAN and Wi-Fi interfaces only) DNS2 IP address.
Default gateway
DefaultGateway
Default gateway IP address.
Additional IP addresses
AdditionalIPAddresses
(LAN interface only) Additional IP addresses of the interface.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.