Join an Organization
An organization is a set of associated user accounts, applications, and resources
that are managed together.
You can make a request to join existing organizations or sub-organization rather than
creating a new one if your colleagues have already created an organization, and you want to
share data, access, or entitlements with each other.
Organization only
: You can browse for public organizations by navigating to the
Organizations
page and selecting Join organization
. When you
browse, you see a list of public organizations created by users with the same email domain
that you are using. It is up to the Administrator or Owner of the organization to make these
organizations visible or not. Private organizations require an invitation. The administrator
or owner of an organization can invite you via email or they can share a join request link
from the Send Invites page in their organization.If you are sent a join request link, the owner or administrator of the organization or
sub-organization will assign your roles on receiving your response to the link
To join an organization:
- From the FactoryTalk Hub menu, selectOrganizations.
- On theOrganizationspage, in the top-right corner selectJoin organization.
- Select an available organization from the list displayed.
- SelectContinue.
To join a sub-organization:
- From the FactoryTalk Hub menu, selectOrganizations.
- Select the parent organization which sub-organization you want to join.
- From the FactoryTalk Hub menu, selectSub-organizations.
- Next to the sub-organization, selectJoin.
The organization or sub-organization administrators receive an
email notification with the access request. By clicking the
Go to Approve
users
button in the email notification, the administrators are redirected to a
FactoryTalk Hub page where they can either approve or dismiss the request. The requestor
receives an email notification when their request was approved or dismissed.Provide Feedback