Elevation view
Elevation
view is a graphical representation of physical Motor
Control Center (MCC) hardware and displays the layout of the lineup as well as specific
device information and status indicators for each device. In
Elevation
view you can:- View multiple lineups simultaneously.
- Change the position of the unit or section within the lineup.
- Import new sections (see FactoryTalk Design Studio Help)
- Export an MCC lineup (see FactoryTalk Design Studio Help)
- Import and viewIntelliCENTER documentation (see FactoryTalk Design Studio Help)
- Start and stop status monitoringStart and stop status monitoring (see FactoryTalk Design Studio Help)to view status indicators for the devices monitored within the lineup.
Provide Feedback