Preface

This publication provides an introduction to
FactoryTalk® Design Studio
that includes:
  • How to get setup in
    FactoryTalk® Hub
    and
    FactoryTalk® Remote Access
    .
  • How to create a project
  • How to add and manage devices
  • How to deploy a project to a controller and go online with a controller.
  • Code generation with
    FactoryTalk® Smart Object
    and
    FactoryTalk®
    Code editor.
For more in-depth information on these topics, see the FactoryTalk® Design Studio Help.
For information on safety application development, see
Develop Safety Applications in
FactoryTalk Design Studio
Programming Manual, publication FTDS-PM001
.
The procedures in this publication use the
FactoryTalk® Design Studio
application. For information about using
Studio 5000 Logix Designer®
software, see
ControlLogix®
5580 and
GuardLogix®
5580 Controllers User Manual, publication 1756-UM543
.
For information about how to use your devices, search the Technical Documentation Center for the user manual for your device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal