SIL Level Match
FactoryTalk®
Design Studio™
validates the Safety
Level set in the Safety Controller Profile against the
safety level of the controller that you are deploying the safety application to. If a SIL level mismatch occurs, an error shows and you cannot deploy the safety
application. You must reconfigure the safety application to match the safety controller
you are deploying to, or deploy the safety application to a controller with a matching
safety configuration.
Provide Feedback