Tasks
Create a task to schedule when programs execute. Schedule a task to run continuously,
periodically, or when triggered by a specific event. A program executes a set of
instructions in a project. Create tasks from the
Execution
explorer,
by either right-clicking on the controller or Tasks
folder and
selecting New Task
.Creating a task varies by task type. Task types include:
- Continuous. A continuous task runs continuously in the background through all assigned programs. CPU times not allocated to other operations scan the assigned programs. After the continuous task scans a program, an output update triggers and the task scans the next program.
- Periodic. Periodic tasks perform a function at a specific rate. Multiple periodic tasks may exist where each task is operates at independent rates.
- Event. Event tasks perform a specific function that is triggered by a specified event.
Create up to 1000 tasks.
FactoryTalk Design Studio Copilot and tasks
When creating a controller, FactoryTalk Design Studio creates a DefaultTask periodic task
with these parameters
- 250 ms Period
- Priority 10
- 500 ms Watchdog
- Inhibit task
- Disable automatic output processing to reduce task overhead OFF.
Use these FactoryTalk Design Studio Copilot prompts with tasks.
- Create a taskPrompt: Create a task Task_001 in CLX_001. (This prompt creates a periodic task. You can specify the type of task to create by using the prompt: Create task Task_001 in CLX_001 as a [type] task).FactoryTalk Design Studio Copilot response: Task_001 in CLX_001 updated from 250 ms to 240 ms.
- Update a taskPrompt: In Task_001 in CLX_001, update the period from 250 ms to 240 ms.FactoryTalk Design Studio Copilot response: Task_001 in CLX_001 updated from 250 ms to 240 ms.
- Delete a taskPrompt: Delete Task_001 in CLX_001.FactoryTalk Design Studio Copilot response: If no programs are in the task that you are deleting, the task deletes. If there is at least one program in this task, FactoryTalk Design Studio informs you that any programs become unscheduled.
- Provide guidance on creating a taskPrompt: How do I create a task in CLX_001?FactoryTalk Design Studio Copilot response: Instructions on how to manually create tasks and examples.
Find information about FactoryTalk Design Studio Copilot prompts for:
Provide Feedback