Editor toolbar
Use the Editor toolbar to carry out common editor functions. The toolbar appears at the
top of each editor in
FactoryTalk®
Design Studio™
. Editor toolbar

This table describes the icons on the toolbar.
Icon | Description |
|---|---|
Indicates the Offline | |
![]() | Opens the tag editor and lists program-scoped tags. |
![]() | Opens the tag editor and lists routine-scoped tags. |
In the Structured Text Editor, opens the
Go-to-line dialog. In the Ladder Editor,
opens the Go-to-rung dialog. Enter a line
number or a rung number in the routine to jump to that
location. | |
Zooms in or out on the display. Another option is to press and
hold CTRL and scroll your mouse wheel. | |
Indicates a syntax error in the routine. |
Provide Feedback