FactoryTalk Smart Object
A
FactoryTalk Smart Object
is an element used to model your system elements and their relationships. For example,
create a FactoryTalk Smart Object
for a tank in a large plant. You can then reuse the
same FactoryTalk Smart Object
for all tanks in the system instead of creating logic for
each tank. A FactoryTalk Smart Object
is also a container that can hold other Smart
Objects, Programs, and Routines. FactoryTalk Smart Object
s support:- Definition and instances
- Behaviors
- Inheritance
- Override
- Containment
Contained programs represent the
ControlLogix
behavior of a FactoryTalk Smart Object
. You can
allocate contained programs to a controller application to then be deployed to a logic
controller. You can modify a
FactoryTalk Smart Object
instance without changing its definition. For
example, you can add additional child FactoryTalk Smart Objects, programs, and tag values
specific to the instance. There are two types of
FactoryTalk Smart Object
instances:- StandaloneFactoryTalk Smart Objects are created in theSystemexplorer and do not have an association with other instances and definitions. Use standaloneFactoryTalk Smart Objects in new projects to test the functionality of the element. You can also use a standaloneFactoryTalk Smart Objectto create a single, non-reusable object.
- FactoryTalk Smart Objects that are instances of a definition inherit behaviors from its definition and any inherited definition in theLibraryexplorer. When updating a definition, all instances and inherited definitions are also updated.
Provide Feedback